The attahed file is an audio recording done on my Nexus4 while being charged on a FOD disabled BQ00410A EVM-085 board. The noise is audible and sequenced. It shows up as soon as a Qi device is placed and charging. Even with the BQ51013EVM-725 and MSP430BQ1010, the same noise is audible, although the magnitude might be different by say, 10% and the sequence might be a little different, but not much in any case. (noise present irrespective of FOD setting, FOD was disabled only for Nexus4)
From my observation, the noise is from the PCBA side, and probably from one or more of the components of the particular bridge rectifier circuit that is active (this being an A6 3Coil board).
Could you please help resolve quickly? We are making a transmitter solution and any audible noise is very detrimental to our product. An OEM is also using TI 410A solution and their circuit has the same issue. Maybe it's just a components/boarding/coating issue, but it is serious. Another chipmaker's solution does not have this issue.
Please help resolve asap.