Hi ,
Can anyone one help to solve following queries?
We are integrating HSR/PRP on AM335x with Quadros. For that we have sample quadros application having quadros_shell to do the ping test. It is using ICSS_EMAC eth configuration.
with DUAL_MAC mode able to do the ping test using PRU 0.
- HSR/PRP able to work on DUAL_MAC mode or we need to configure to SWICH mode? (we tried with changing it to SWITCH mode and then we are not able to do the ping test)
- What are the basic needs of HSRPRP to work on Quadros. (Currently we have PRU-ICSS-HSR-PRP-DAN-01.00.05.01-Linux-x86-Install.bin and pdk 1.0.12)
- Do we need to integrate SNMP to work with HSR PRP ?