This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXIDK5718: Can AM5728/AM5748 work on the TMDXIDK5718 board?

Part Number: TMDXIDK5718
Other Parts Discussed in Thread: AM5726, AM5746, AM5716, AM5728, AM5718, AM5748,

Hi Ti

AM571x,AM572x,AM574x have the same footprint->FCBGA (760)

We know most HW Function is the same (HDMI and LCD Interface are different and others).

The difference is inside. Such as  EVE Analytic Processors, CPU Frequency. 

My question is:

Whether AM5746 backward compatible AM5726,AM5726 backward compatible AM5716? ( HW function and Ball definition backward-compatible ).

Same question: Whether AM5748 backward compatible AM5728,AM5728 backward compatible AM5718?

For example:

For IDK EVM Board-> TMDXIDK5718

If we replace CPU from  AM5718  to AM5728/AM5748 Without Re-lay?

Of cause, we need to evaluate the power Consumption and thermal and re-build the SDK

But If we just review Ball Pins compatibility and Function, Is AM5728、AM5748 workable on the TMDXIDK5718 board?  Whether all EVM functions are workable?  

Foxconn Qin