Other Parts Discussed in Thread: AM5726, AM5746, AM5716, AM5728, AM5718, AM5748,
Hi Ti
AM571x,AM572x,AM574x have the same footprint->FCBGA (760)
We know most HW Function is the same (HDMI and LCD Interface are different and others).
The difference is inside. Such as EVE Analytic Processors, CPU Frequency.
My question is:
Whether AM5746 backward compatible AM5726,AM5726 backward compatible AM5716? ( HW function and Ball definition backward-compatible ).
Same question: Whether AM5748 backward compatible AM5728,AM5728 backward compatible AM5718?
For example:
For IDK EVM Board-> TMDXIDK5718
If we replace CPU from AM5718 to AM5728/AM5748 Without Re-lay?
Of cause, we need to evaluate the power Consumption and thermal and re-build the SDK
But If we just review Ball Pins compatibility and Function, Is AM5728、AM5748 workable on the TMDXIDK5718 board? Whether all EVM functions are workable?
Foxconn Qin