This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSIDK572: TMDSIDK572: TMDSIDK572 GPMC interface read and write issue

Part Number: TMDSIDK572


Hi team, 

            We are using TMDSIDK572 – AM572x Industrial Development Kit (IDK). In this IDK there is no default GPMC interface. We are using "fpga read write - async mode" bare metal as-is. when we perform write and read operation individually i am getting data properly and got clock signal in oscilloscope. but we we perform read after write in continuously, first we read proper data and after write operation we will miss read data. please check and support us. here i attached my baremetal file and read and operation scanrio. and also i couldn't see any value in memory window which i write through GPMC bus.

            I am using this SDK "ti-processor-sdk-rtos-am57xx-evm-06.03.00.106-Windows-x86-Install" for windows. there is no default driver available for GPMC bus. So, we are using CSL example GPMC code

.

/*
 *  Copyright (C) 2013-2019 Texas Instruments Incorporated - http://www.ti.com/
 *
 *  Redistribution and use in source and binary forms, with or without
 *  modification, are permitted provided that the following conditions
 *  are met:
 *
 *    Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 *    Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the
 *    distribution.
 *
 *    Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
 *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
 *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
 *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
 *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
 *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
 *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
 *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
 *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
 *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
 *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 *
 */
/**
 *   \file    main.c
 *
 *   \brief   GPMC test application optimized for FPGA read and write using CPU and DMA.
              Use the macros to select between synchronous/non-synchronous,
              burst/non-burst, and CPU/DMA modes. The application will perform
              reads and writes and output the benchmarks to UART terminal. The
              test will pass/fail depending on whether the benchmark numbers fall
              within the predefined bounds.
              The timing values configured in GPMC_init() can be tuned to further
              optimize your application.

              One of the following configurations can be tested at a time by defining/undefining the macros below.
              1. Synchronous Burst DMA Mode
              2. Synchronous Non-burst DMA Mode
              3. Asynchronous Burst DMA Mode
              4. Asynchronous Non-burst DMA Mode
              5. Synchronous Burst CPU Mode
              6. Synchronous Non-burst CPU Mode
              7. Asynchronous Burst CPU Mode
              8. Asynchronous Non-burst CPU Mode
 *
 */
/* ========================================================================== */
/*                             Include Files                                  */
/* ========================================================================== */
//NEW ADDED BY GPIO BAREMETAL
#include <ti/board/board.h>

#include <ti/csl/example/utils/uart_console/inc/uartConfig.h>
#include <ti/csl/csl_gpmc.h>
#include <ti/csl/soc.h>
#include <ti/csl/hw_types.h>
#include <ti/csl/csl_edma.h>
#include <ti/csl/example/edma/edma_test/sample.h>

/* ========================================================================== */
/*                                 Macros                                     */
/* ========================================================================== */
/* ========================================================================== */
/*                             Include Files                                  */
/* ========================================================================== */

//#define BURST_MODE
//#define SYNC_MODE

/* ========================================================================== */
/*                            Global Variables                                */
/* ========================================================================== */

signed char __attribute__((section(".my_sect_ddr"))) _srcBuff1[MAX_BUFFER_SIZE];
signed char __attribute__((section(".my_sect_ddr"))) _dstBuff1[MAX_BUFFER_SIZE];

uint32_t edma_ch_num = 1;
uint32_t edma_tcc_num = 1;
uint32_t edma_evtq_num = 0;

uint32_t region = EDMA3_CC_REGION;

signed char *srcBuff1;
signed char *dstBuff1;

extern uint32_t base_address;

/*To use UARTConfigPuts function for prints*/
uint32_t uartBaseAddr = SOC_UART3_BASE;

/* To use for benchmarking */
#define TIMER14_TCLR (*((volatile uint32_t *)0x4882A038))
#define TIMER14_TLDR (*((volatile uint32_t *)0x4882A040))
#define TIMER14_TCRR (*((volatile uint32_t *)0x4882A03C))
#define TIMER14_TMAR (*((volatile uint32_t *)0x4882A04C))
#define TIMER14_TSICR (*((volatile uint32_t *)0x4882A054))
/* ========================================================================== */
/*                          Function Definitions                              */
/* ========================================================================== */
void GPMC_init(void);
void padConfig_prcmEnable(void);

int main(void)
 {

    uint32_t i, t_start, t_stop, t_overhead;

#ifdef DMA_ENABLE
    uint32_t t_delta_dma_writes, t_delta_dma_reads;
#else
    uint32_t t_delta_cpu_writes, t_delta_cpu_reads;
    volatile uint16_t var0 = 0xFFFFF;
    uint16_t temp_delay=0;
    volatile uint32_t * GPMC0 = (volatile uint32_t*) 0x0800000C;

    volatile uint32_t * GPMC1 = (volatile uint32_t*) 0x08000004;
    /*  volatile uint32_t * GPMC2 = (volatile uint32_t*) 0x08000008;
    volatile uint32_t * GPMC3 = (volatile uint32_t*) 0x0800000C;
    volatile uint32_t * GPMC4 = (volatile uint32_t*) 0x08000010;
    volatile uint32_t * GPMC5 = (volatile uint32_t*) 0x08000014;
    volatile uint32_t * GPMC6 = (volatile uint32_t*) 0x08000018;
    volatile uint32_t * GPMC7 = (volatile uint32_t*) 0x0800001C;*/
#endif
    /*MMC1 PAD Configuration*/
    UARTConfigInit(uartBaseAddr, BAUD_RATE_115200, UART_WORD_LENGTH_8,UART_STOP_BIT_1, UART_NO_PARITY, UART_16x_MODE);
    UARTConfigPuts(uartBaseAddr, "\nUART INIT DONE\n", -1);

    padConfig_prcmEnable();
    GPMC_init();

    while(1)
    {

            var0 = *GPMC0;
            UARTConfigPuts(uartBaseAddr, "\nDATA =", -1);
            UARTConfigPutNum(uartBaseAddr,(var0&0x03));
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);

           *GPMC1 = 0xFD;
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);
            for(temp_delay=0;temp_delay<65000;temp_delay++);

    }

    return 0;
}

/* Configures GPMC registers with timing values optimized for an FPGA */
void GPMC_init(void)
{
    uint32_t baseAddr = CSL_MPU_GPMC_CONF_REGS_REGS;
    uint32_t config;
    uint16_t temp_delay=0;
    //GPMC reset
    GPMCModuleSoftReset(baseAddr);

    for(temp_delay=0;temp_delay<65000;temp_delay++);

    //while(!GPMCModuleResetStatusGet(baseAddr));

    /* Enable the chip select */
       GPMCCSConfig(baseAddr, GPMC_CHIP_SELECT_0, GPMC_CS_DISABLE);

    /* Select the chip-select base address, chip addr needs to be given */
    GPMCBaseAddrSet(baseAddr, GPMC_CHIP_SELECT_0, 0x00000008);

    /* Select the chip-select mask address */
    GPMCMaskAddrSet(baseAddr, GPMC_CHIP_SELECT_0, GPMC_CS_SIZE_64MB);

    /* Set the device size attached */
    GPMCDevSizeSelect(baseAddr, GPMC_CHIP_SELECT_0, GPMC_DEVICESIZE_16BITS);

    /* Set the read mode operation and write mode operation */
#ifdef SYNC_MODE
    GPMCReadTypeSelect(baseAddr, GPMC_CHIP_SELECT_0, GPMC_READTYPE_SYNC);
    GPMCWriteTypeSelect(baseAddr, GPMC_CHIP_SELECT_0, GPMC_WRITETYPE_SYNC);
#else
    GPMCReadTypeSelect(baseAddr,GPMC_CHIP_SELECT_0, GPMC_READTYPE_ASYNC);
    GPMCWriteTypeSelect(baseAddr,GPMC_CHIP_SELECT_0, GPMC_WRITETYPE_ASYNC);
#endif

    /* Select single access or multiple access reads and writes*/
#ifdef BURST_MODE
    GPMCAccessTypeSelect(baseAddr, GPMC_CHIP_SELECT_0, GPMC_MODE_READ,
    GPMC_ACCESSTYPE_MULTIPLE);
    GPMCAccessTypeSelect(baseAddr, GPMC_CHIP_SELECT_0, GPMC_MODE_WRITE,
    GPMC_ACCESSTYPE_MULTIPLE);
#else
    GPMCAccessTypeSelect(baseAddr, GPMC_CHIP_SELECT_0, GPMC_MODE_READ, GPMC_ACCESSTYPE_SINGLE);
    GPMCAccessTypeSelect(baseAddr, GPMC_CHIP_SELECT_0, GPMC_MODE_WRITE, GPMC_ACCESSTYPE_SINGLE);
#endif

    /* Set the signals timing latencies scalar factor */
    GPMCTimeParaGranularitySelect(baseAddr, GPMC_CHIP_SELECT_0,
    GPMC_TIMEPARAGRANULARITY_X1);

    /* Set the address and data multiplexed protocol */
    GPMCAddrDataMuxProtocolSelect(baseAddr, GPMC_CHIP_SELECT_0,
    GPMC_MUXADDDATA_NOMUX);

    /* Set the timing parameters for the chip select signal */
    //CSWROFFTIME, CSRDOFFTIME, CSEXTRADELAY, CSONTIME
    config = GPMC_CS_TIMING_CONFIG(10, 7, GPMC_CS_EXTRA_NODELAY, 0);
    GPMCCSTimingConfig(baseAddr, GPMC_CHIP_SELECT_0, config);

    /* Set the timing parameters for the ADV# signal */
    /* ADVAADMUXWROFFTIME, ADVAADMUXRDOFFTIME, ADVWROFFTIME, ADVRDOFFTIME, ADVEXTRADELAY, ADVAADMUXONTIME, ADVONTIME */
    config = GPMC_ADV_TIMING_CONFIG(0, 0, 4, 4, GPMC_ADV_EXTRA_NODELAY, 0, 0);
    GPMCADVTimingConfig(baseAddr, GPMC_CHIP_SELECT_0, config);

    /* Set the timing parameters for the WE# and OE# signals */
    /* WEOFFTIME, WEEXTRADELAY, WEONTIME, OEAADMUX_OFFTIME, OEOFFTIME, OEEXTRADELAY, OEAADMUX_ONTIME, OEONTIME */
    config = GPMC_WE_OE_TIMING_CONFIG(7, 0, 4, 0, 7, GPMC_OE_EXTRA_NODELAY, 0,
                                      4);
    GPMCWEAndOETimingConfig(baseAddr, GPMC_CHIP_SELECT_0, config);

    /* Set the RdAccessTime and CycleTime timing parameters */
    /* RDCYCLETIME, WRCYCLETIME, RDACCESSTIME, PAGEBURSTACCESSTIME */
    config = GPMC_RDACCESS_CYCLETIME_TIMING_CONFIG(9, 9, 6, 3);
    GPMCRdAccessAndCycleTimeTimingConfig(baseAddr, GPMC_CHIP_SELECT_0, config);

    /* Configure the Cycle2Cycle and BusTurnAround timing parameters */
    /* CYCLE2CYCLEDELAY, CYCLE2CYCLEDELAYSAMECSCFG, CYCLE2CYCLEDELAYDIFFCSCFG, BUSTATIME */
    config = GPMC_CYCLE2CYCLE_BUSTURNAROUND_TIMING_CONFIG(
            2, GPMC_CYCLE2CYCLESAMECSEN_C2CDELAY,
            GPMC_CYCLE2CYCLEDIFFCSEN_NOC2CDELAY, 0);
    GPMCycle2CycleAndTurnArndTimeTimingConfig(baseAddr, GPMC_CHIP_SELECT_0,
                                              config);

    /* Configure the WrAccessTime, Cycle2Cycle andBusTurnAround timing parameters.*/
    /* WRACCESSTIME, WRDATAONADMUXBUS */
    GPMCWrAccessAndWrDataOnADMUXBusTimingConfig(baseAddr, GPMC_CHIP_SELECT_0, 6,
                                                4);

    /* Set the FCLK divide down value */
    GPMCFclkDividerSelect(baseAddr, GPMC_CHIP_SELECT_0, GPMC_FCLK_DIV_BY_4);

    /* Set the attached device page (burst) length */
    GPMCDevPageLenSet(baseAddr, GPMC_CHIP_SELECT_0,
    GPMC_DEV_PAGELENGTH_SIXTEEN);

    /* Enable the chip select */
    GPMCCSConfig(baseAddr, GPMC_CHIP_SELECT_0, GPMC_CS_ENABLE);

    //GPMC reset
  //  GPMCModuleSoftReset(baseAddr);
  //  while(!GPMCModuleResetStatusGet(baseAddr));
}


void padConfig_prcmEnable(void)
{
    Board_initCfg boardCfg;
     boardCfg = BOARD_INIT_UNLOCK_MMR | BOARD_INIT_UART_STDIO |
                BOARD_INIT_MODULE_CLOCK | BOARD_INIT_PINMUX_CONFIG;
     Board_init(boardCfg);
     HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD0,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD1,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD2,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD3,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD4,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD5,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD6,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD7,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD8,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD9,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD10,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD11,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD12,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD13,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD14,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD15,0x00050000);



        /*GPMC Add lines A0-A27*/
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A0,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A1,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A2,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A3,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A4,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A5,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A6,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A7,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A8,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A9,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A10,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A11,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A12,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A13,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A14,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A15,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A16,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A17,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A18,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A19,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A20,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A21,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A22,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A23,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A24,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A25,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A26,0x00000000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A27,0x00000000);
        /*GPMC chip select*/
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_CS0,0x00020000);

        /*GPMC control lines*/
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_ADVN_ALE,0x00020000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_OEN_REN,0x00030000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_WEN,0x00030000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_BEN0,0x00030000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_WAIT0,0x0000000F);
//        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_CLK,0x00060000);

#if 0
     /*Pad configurations */
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_UART3_RXD,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_UART3_TXD,
            0x00000000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_UART2_CTSN,
            0x00060002);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_UART2_RTSN,
            0x00060001);
    /*Pad configurations*/
    /*GPMC Data lines AD0-AD15*/
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD0,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD1,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD2,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD3,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD4,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD5,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD6,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD7,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD8,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD9,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD10,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD11,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD12,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD13,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD14,
            0x00050000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD15,
            0x00050000);
    /*GPMC Add lines A0-A27*/
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A0,
            0x00000000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A1,
            0x00000000);//0x00040000
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A2,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A3,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A4,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A5,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A6,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A7,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A8,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A9,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A10,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A11,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A12,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A13,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A14,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A15,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A16,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A17,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A18,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A19,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A20,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A21,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A22,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A23,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A24,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A25,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A26,
            0x00040000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A27,
            0x00040000);

    /*GPMC chip select*/
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_CS0,
            0x00060000);
    /*GPMC control lines*/
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_ADVN_ALE,
            0x00060000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_OEN_REN,
            0x00030000);//0x00030000
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_WEN,
            0x00060000);
    HW_WR_REG32(
            CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_BEN0,
            0x00070000);
    HW_WR_REG32(
               CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_BEN1,
               0x00070000);
    HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_WAIT0, 0x0000000F);
    HW_WR_REG32(      CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_CLK,   0x00060000);

#endif

}
/***************************** End Of File ***********************************/