This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4VM GPIO OUT level over load current

Part Number: TDA4VM

The TDA4VM dig output pin for VCC 3.3V is specified in table 7-9 to be for low level worst case 0.4V and for high level worst case 2.4V.  According to the table description this is over the full range, so full load current and full temp. 

Do we have chart of the low and high levels versus the load current.? My customer is using a logic behind the out pin that would be violated with the 0.4V and 2.4V levels, but it is driving <=1mA instead of the allowed 5 and 6mA.