I've already asked 2 questions connected with running darknet with OpenCL on BeagleBone AI AM5729 Debian image (am57xx-eMMC-flasher-debian-10.9-lxqt-tidl-armhf-2021-05-28-6gb.img.xz) from (https://rcn-ee.net/rootfs/bb.org/testing/2021-05-28/) and I handled previous issues :
- TIOCL WARNING: Opening Linux shared memory: No such file or Directory.
- TIOCL FATAL: The TI Multicore Tools daemon (/usr/bin/ti-mctd) is not running. To start daemon, rm /dev/shm/HeapManager (if exists); ti-mctd. Re-run application. Refer User Guide for details. Aborted
And then I had one more : ti-mct-daemon.service does not exist.
I installed darknet with guide from isowa (https://iblog.isowa.io/2020/04/29/darknet-in-opencl-on-beagleboard-ai/), however I did not installed extra packages, only ocl-icd-opencl-dev and in src/opencl.h wrote #define CL_TARGET_OPENCL_VERSION 120 .
Then I called my custom nn YOLOv4 with sudo ./darknet detector test..... And have a new issue : opencl_init: could not get device IDs. I really need help badly, tried to find answer in the internet, however I failed in my attempts.
Hope to get answer really fast.