Hi, I am seemingly unable to run the scripts to install the SDK and PDK for the AM437X ,
PROCESSOR-SDK-RTOS-AM437X_06.03.00.106,
Result from setupenv.bat
Environment Configuration:
***************************************************
SDK_INSTALL_PATH : C:\ti
PDK_INSTALL_PATH : C:/ti/pdk_am437x_1_0_17/packages
GMAKE_INSTALL_PATH : C:/ti/xdctools_3_55_02_22_core
PDK_SOC : am437x
PDK_VERSION : 1_0_17
RULES_MAKE : C:/ti/pdk_am437x_1_0_17/packages/ti/build/Rules.make
***************************************************
IPC_PLATFORM: UNKNOWN
IPC_ALT_PLATFORM:
PROC_SDK_INSTALL_PATH : C:/ti/processor_sdk_rtos_am437x_6_03_00_106
**************************************************************************
Changing to short name to support directory names containing spaces
current directory: C:/ti/processor_sdk_rtos_am437x_6_03_00_106
PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED
**************************************************************************
Result from executing gmake:
C:\ti\processor_sdk_rtos_am437x_6_03_00_106>gmake
C:\ti/xdctools_3_55_02_22_core/gmake pdk
gmake[1]: Entering directory 'C:/ti/processor_sdk_rtos_am437x_6_03_00_106'
C:\ti/xdctools_3_55_02_22_core/gmake -C C:/ti/pdk_am437x_1_0_17/packages all
gmake[2]: Entering directory 'C:/ti/pdk_am437x_1_0_17/packages'
C:\ti/xdctools_3_55_02_22_core/gmake -C C:/ti/pdk_am437x_1_0_17/packages/ti/build -f makefile all CORE=a9host BOARD=evmAM437x SOC=am437x BUILD_PROFILE=release; C:\ti/xdctools_3_55_02_22_core/gmake -C C:/ti/pdk_am437x_1_0_17/packages/ti/build -f makefile all CORE=a9host BOARD=idkAM437x SOC=am437x BUILD_PROFILE=release; C:\ti/xdctools_3_55_02_22_core/gmake -C C:/ti/pdk_am437x_1_0_17/packages/ti/build -f makefile all CORE=a9host BOARD=skAM437x SOC=am437x BUILD_PROFILE=release;
C:/Users/krazy/AppData/Local/Temp/make7276-1.sh: 1: C:/Users/krazy/AppData/Local/Temp/make7276-1.sh: C:ti/xdctools_3_55_02_22_core/gmake: not found
C:/Users/krazy/AppData/Local/Temp/make7276-1.sh: 1: C:/Users/krazy/AppData/Local/Temp/make7276-1.sh: C:ti/xdctools_3_55_02_22_core/gmake: not found
C:/Users/krazy/AppData/Local/Temp/make7276-1.sh: 1: C:/Users/krazy/AppData/Local/Temp/make7276-1.sh: C:ti/xdctools_3_55_02_22_core/gmake: not found
gmake[2]: *** [makefile:87: buildinfra_all] Error 127
gmake[2]: Leaving directory 'C:/ti/pdk_am437x_1_0_17/packages'
gmake[1]: *** [makefile:84: pdk] Error 2
gmake[1]: Leaving directory 'C:/ti/processor_sdk_rtos_am437x_6_03_00_106'
gmake: *** [makefile:58: all_libs] Error 2
gmake starts running however seemingly a typo is there when trying to execute it later, it should be C:/ti not C:ti
I'm unsure which script or makefile is causing this
Thanks