Hi,
My customer is looking for a power supply adapter for TMDSDSK6713.
Is the following correct?
DC supply 5V
Outer 5.5mm
Inner 2.5mm
Center plus
Regards,
Rei
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer is looking for a power supply adapter for TMDSDSK6713.
Is the following correct?
DC supply 5V
Outer 5.5mm
Inner 2.5mm
Center plus
Regards,
Rei
Hi Rei,
Apologies in advance for the long delay. Yes, you are correct, power (+5 volts) is brought onto the TMS320C6713 DSK via the J5 connector. The connector has an outside diameter of 5.5 mm. and an inside diameter of 2.5 mm.
Regards,
Mike