Hi,
I'm trying to develop my own design based on TMDSICE3359 but the memory layout of Flash chips is causing some questions. I have erased the Beckhoff sw from the SPI Flash and I think I don't need such memory chip at all. And I don't need a Board ID Eeprom either due to only one possible board design and there will be only one dtb file in /boot of Linux rootfs. But I don't know should I have a NOR Flash in the design. Does the NOR Flash contain any part of the U-boot in the TMDSICE3359 design or does the FAT32 partition of the SD card contain all the U-boot?
I have a plan to have only an eMMC Flash in my design but if I need also a SD card connection for sw update in the production line, should these two use different MMC buses of AM335x? I think I could try to use some of the methods mentioned in https://e2e.ti.com/support/processors-group/processors/f/processors-forum/904467/processor-sdk-am335x-emmc-programming?tisearch=e2e-sitesearch&keymatch=am335x%20emmc%20programming for uploading the sw to the eMMC.
Regards,
Jani