This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: No Matrix App appeared on SDK 7.3.0.5

Part Number: PROCESSOR-SDK-AM335X

Hi TI

I tried to setup PROCESSOR-SDK_LINUX_7.3.0.5 running on top of AM335x Starter Kit.

It was able to boot up with SDK 6.0 image which was already flashed from factory.  It works fine. 

And I flashed the pre-built binary of "am335x_evm_linux_7.3.0.5.img" into a new uSD card. It able to boot up. But Matrix UI screen not appeared as below.

Can you please let me know why Matrix UI does not work on SDK 7.3

At the end of booting, Both board able to root login to the board without hang. But No matrix UI works for new SDK..