The initial value of GPMC_CONFIG1_i [DEVICETYPE] is "0h: NOR flash-like".
GPMC_NAND_COMMAND_i resulted in an error when running the TMDS64GPEVM evaluation board with GPMC defaults.
(1) Why does a NAND error occur even though DEVICETYPE is the default NOR?
(2) Please tell me the setting value that does not cause GPMC error on the TMDS64GPEVM evaluation board.
==GPMC register of TMDS64GPEVM evaluation board==
--GPMC initial value
GPMC_CONFIG1: 00000000h (CS1-3 is 00001000h)
GPMC_CONFIG2: 00101001h
GPMC_CONFIG3: 22060514h
GPMC_CONFIG4: 10057016h
GPMC_CONFIG5: 010F1111h
GPMC_CONFIG6: 8F070000h
GPMC_CONFIG7: 00000F40h (CS1-3 is 00000F00h)
--GPMC error register
GPMC_ERR_TYPE [ERRORVALID]: 1h
GPMC_ERR_TYPE [ERRORNOTSUPPADD]: 1h
GPMC_ERR_TYPE [ILLEGALMCMD]: 2h
GPMC_ERR_ADDRESS: 7B00013Ch (*)
(*) A30 : 1h = for GPMC register region
A29-0: 3B00013Ch = GPMC_NAND_COMMAND_i