Hello,
(You know CCS is being used for large projects... yes?)
How about a way to STOP a build all? Like a big project that takes in excess of 30 minutes to build, and it's necessary to stop it due to some issue...? The only option I can find is to violently kill it in the task manager,
Good coding techniques mean can be encapsulating common functionality in common subfolders, not in one massive 15K line single source code file...
So, how about a way to "Build Files in Selected Folder" rather than just "Build Selected File" ? That way someone can simply build all the files in one folder which represents added or updated functions that are across maybe 10 source files.
Just some suggestions to make life easier.
-CSW