Hello TI,
Are there internal diode protection clamps on the RMII_MHZ_50_CLK pin of the TMS320C6748, and if so, what is the maximum I_k clamp diode current, please?
We expect to see a clamp diode to DVDD3318 but initial measurements seem to indicate no diode clamps on this pin - is this correct?
If there are no clamp diodes, what is the max pin voltage allowable with the relevant DVDD3318 = 1.8V?