Other Parts Discussed in Thread: TPS659037
Hello
Regarding the power startup of TMDXIDK5718,
Is there a way to turn on the power without pressing POWER ON SW (SW3)?
KOUSUKE AYAORI
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
Regarding the power startup of TMDXIDK5718,
Is there a way to turn on the power without pressing POWER ON SW (SW3)?
KOUSUKE AYAORI
Hi,
As per board design that is needed. I am not sure if you can do a Power-On without board modifications if that is not to be used,
Are you facing issues with that?
- Keerthy
HELLO
We are proceeding with the circuit design with reference to TMDXIDK5718.
I want to design so that the power can be turned on without pressing POWER ON SW.
The TMDXIDK5718 schematic page 5 has comments regarding population options for pushbutton or automatic start (R18 is populated, R931 is open for pushbutton start. For automatic start, R18 is open and R931 is populated). This is also discussed in TPS659037 User Guide (sliu011f.pdf)