Hi everybody ,
in production I m moving from micron DDR3 to ISSI
MICMT41K128M16JT-107 IT:K
IS43TR16128DL-107MBLI
they are pin2pin and I used app note getting numbers hereunder :
My question is : can I use ONLY Micron values ( so to have only 1 binary for all my boards , no matter DDR3 in use ) ?
ISSI values are in Micron range , but not the optimal one , is it an issue ?
ISSI:
***************************************************************
The Slave Ratio Search Program Values are...
***************************************************************
PARAMETER MAX | MIN | OPTIMUM | RANGE
***************************************************************
DATA_PHY_RD_DQS_SLAVE_RATIO 0x06c | 0x005 | 0x038 | 0x067
DATA_PHY_FIFO_WE_SLAVE_RATIO 0x1c1 | 0x050 | 0x108 | 0x171
DATA_PHY_WR_DQS_SLAVE_RATIO 0x10a | 0x031 | 0x09d | 0x0d9 ??????
DATA_PHY_WR_DATA_SLAVE_RATIO 0x14a | 0x071 | 0x0dd | 0x0d9 ????
***************************************************************
vs Micron:
***************************************************************
DATA_PHY_RD_DQS_SLAVE_RATIO 0x06d | 0x004 | 0x038 | 0x069
DATA_PHY_FIFO_WE_SLAVE_RATIO 0x1bd | 0x049 | 0x103 | 0x174
DATA_PHY_WR_DQS_SLAVE_RATIO 0x0f1 | 0x013 | 0x082 | 0x0de
DATA_PHY_WR_DATA_SLAVE_RATIO 0x131 | 0x053 | 0x0c2 | 0x0de
***************************************************************
any suggestion ?thank you
BR
Carlo