I just installed code composer 10.4 on Ubuntu 18.04. I downloaded the full installer and selected the "C55x ultra-low-power DSP" component. The installer ran without a hitch, but when I go to create a new CCS project for the target C551x, CCS tells me 'No compilers are currently installed for this device-family. Click 'View > CCS App Center' to install a compiler before creating a project for this device.' I then go there and select the C5500 Compiler, but when I hit "Install Software" I get a dialog saying "Failed to install the selected add-ons. Please see error log file ...". On the "Eclipse log" I get an error that might be relevant, but I could be mistaken:
!ENTRY org.eclipse.equinox.event 4 0 2021-07-14 11:13:33.163
!MESSAGE Exception while dispatching event org.osgi.service.event.Event [topic=org/eclipse/e4/ui/model/application/ApplicationElement/tags/ADD] {ChangedElement=org.eclipse.e4.primaryDataStack=org.eclipse.e4.ui.model.application.ui.basic.impl.PartStackImpl@5a23b9d1 (tags: [org.eclipse.e4.primaryDataStack, EditorStack, active, Maximized], contributorURI: null) (widget: CTabFolder {}, renderer: org.eclipse.e4.ui.workbench.renderers.swt.StackRenderer@68dbe225, toBeRendered: true, onTop: false, visible: true, containerData: null, accessibilityPhrase: null), org.eclipse.e4.data={ChangedElement=org.eclipse.e4.primaryDataStack=org.eclipse.e4.ui.model.application.ui.basic.impl.PartStackImpl@5a23b9d1 (tags: [org.eclipse.e4.primaryDataStack, EditorStack, active, Maximized], contributorURI: null) (widget: CTabFolder {}, renderer: org.eclipse.e4.ui.workbench.renderers.swt.StackRenderer@68dbe225, toBeRendered: true, onTop: false, visible: true, containerData: null, accessibilityPhrase: null), AttName=tags, EventType=ADD, Position=3, Widget=CTabFolder {}, NewValue=Maximized}, AttName=tags, EventType=ADD, Position=3, Widget=CTabFolder {}, NewValue=Maximized} to handler org.eclipse.e4.ui.internal.di.UIEventObjectSupplier$UIEventHandler@609f136b
!STACK 0
org.eclipse.e4.core.di.InjectionException: java.lang.IllegalArgumentException:
at org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:68)
at org.eclipse.e4.ui.internal.di.UIEventObjectSupplier$UIEventHandler.lambda$0(UIEventObjectSupplier.java:64)
at org.eclipse.swt.widgets.Synchronizer.syncExec(Synchronizer.java:236)
at org.eclipse.ui.internal.UISynchronizer.syncExec(UISynchronizer.java:146)
at org.eclipse.swt.widgets.Display.syncExec(Display.java:5786)
at org.eclipse.e4.ui.internal.workbench.swt.E4Application$1.syncExec(E4Application.java:219)
at org.eclipse.e4.ui.internal.di.UIEventObjectSupplier$UIEventHandler.handleEvent(UIEventObjectSupplier.java:64)
I read on a similar post that somebody suggested trying to manually install the addon, but the link to the solution was broken. Is there any way to do that? Or is there any other workaround? I found some other relevant posts, but no solution or workaround seem to apply to my case
Thanks