Hi Everyone,
For TMDSIDK574 board, i have built GPIO_LedBlink_ldkAM574x_armTestProject project using SOC-AM574x and idkAM574x board. Project successfully imported in CCS v9.3.
While running this project there is no SD card inserted in board nor any OS is running.
While building project, i have selected project properties as
Variant -AM574x-Cortex A15
AM574x[Cortex-A]
Connection - Texas Instrument XDS 100V2 USB Debug
Connected with J19 of TMDSIDK574 board.
I am facing two problem with this project
1) Sometime while building project,it's giving error as
Description Resource Path Location Type
/home/iveer5/ti/RTOS/pdk_am57xx_1_0_17/packages/ti/boot/sbl/tools/scripts/AM57xImageGen.sh: line 37: mono: command not found GPIO_LedBlink_idkAM574x_armTestProject C/C++ Problem
What does it mean?
2) If i will build 2-3 times, then those error will not pop up and at that time if will try to debug, it will show me Load program error as
CortexA15_0: File Loader: Verification failed: Values at address 0x80000000 do not match Please verify target memory and memory map.
CortexA15_0: GEL: File: /home/iveer5/workspace_v9/GPIO_LedBlink_idkAM574x_armTestProject/Debug/GPIO_LedBlink_idkAM574x_armTestProject.out: a data verification error occurred, file load failed.
CortexA15_0: Unable to terminate memory download: NULL buffer pointer at 0x3aa4 (Emulation package 9.3.0.00042)
Can someone please suggest me how to tackle this?
I have also seen RTOS/AM5746: How to build/debug "boot.asm" by CCS in PROCESSOR-SDK-RTOS-AM57X, but i am unable to select boot.asm file. Because there is not boot file for Cortex-A15.
In my installed directory(bios_6_76_03_01/packages/gnu/targets/arm), its only available for
- rtsv5T
- rtsv6
- rtsv7A
- rtsv7M
- rtsv8A
- rtsv8M
Please help me to run GPIO project on the board.
Thanks & Regards,
Divyesh