Other Parts Discussed in Thread: TPS62361B, TPS62362, DRA718, DRA752, LP8733
Hello,
I'm trying to get the TPS62361B working in combination with the AM5708 in u-boot. We have a total of 3 devices (i2c1, i2c3 and i2c4) connected.
There is a tps62362 driver available. But it looks like it has a slightly different interface to the lp873x driver we are currently using. There is also no mention of it in the configuration (Kconfig). Is this an older to be set to tobsolete driver perhaps?
I also found some defines regarding the tps62361 in "arch/arm/include/asm/arch-omap5/clock.h" which seems to imply a different way of using the device then the lp87x which uses configuration data from the device tree.
My question is what is the quickest way to get the TPS62361B working under u-boot? Out u-boot is based on a ti2019.04 tag. Should I use existing code or just plain send i2c commands to the devices over the i2c buses?
Kind regards,
Johan