This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSIDK437X: Read and write TLK105L registers.

Part Number: TMDSIDK437X
Other Parts Discussed in Thread: TLK105L, TLK105

Hello.

1. I use NIMU_BasicExample_idkAM437x_armExampleproject. How can I read and write registers of TLK105L? For my project on my board, I will need my own settings. How can i do this? Is there a driver with which you can control the PHY chip?

2. In NIMU_BasicExample_idkAM437x_armExampleproject work only one port - PRU0. Is it right? If I change at CfgAddEntry item value of new entry from 1 to 2, then work port 2 - PRU1. Is that how it should be? If so, how can I make both ports work with different IPs?

Regards, Dmitry.