Hi:
Sorry to keep dribbling this in.
I am at this step:
software-dl.ti.com/.../Overview_Building_the_SDK.html
$ ./oe-layertool-setup.sh -f configs/core-sdk/core-sdk-<version>-config.txt
but the only file that looks close is this one.
coresdk-08.00.00.004-config.txt
However, here
software-dl.ti.com/.../Release_Specific_Yocto_layer_Configuration.html
it says to use this one
processor-sdk-08.00.00.21-config.txt
Which coresdk file should I use? Or should I be using the processor-sdk file?
I'm not one for trial and error with yocto, so it would be good if this stuff was specfied.
Thanks
Howard