Hi all. I've been spelunking through all the source code in my ~/ti/* tree looking for low-level functions to support porting my code from another processor to the TDXICE110. I'm designing a board using this ICE as a model, and adding I/O and a few other features.
I have an existing code base based on the Beckhoff SSC code, and it mostly fits right in to the TI SSC-derived code. I'm using the RTOS based system, since for a future application this will be handy, but for this first product, a simple single-loop application works fine.
In our init code, I need to have a microsecond-level timer (spin-loop is fine) for reading a 1-wire EEPROM using bit-banging. Is there such a thing somewhere in the voluminous code samples and drivers?
Hints on where to find this kind of information in code or documents would be most welcome!
Thanks!
John