Hi, dear experts,
We want to enableTI’s inline ECC for DDR when DDR size is 3GB, could you give me some guidance about this?
Best Reagrds
Nathan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, dear experts,
We want to enableTI’s inline ECC for DDR when DDR size is 3GB, could you give me some guidance about this?
Best Reagrds
Nathan
Nathan,
When you say 3GB is it 3GB out of 4 GB or it is that your DDR size itself is 3GB?
I believe we have communicated that Inline ECC when enabled will be for entire DDR. Hence the question.
- Keerthy
Nathan,
I believe you already have the 2GB inline ECC enabling patches.
inline-ecc-2GB.tar
Original code changes:
diff --git a/board/ti/j721e/evm.c b/board/ti/j721e/evm.c index d9846f3c46..8f4768f1a2 100644 --- a/board/ti/j721e/evm.c +++ b/board/ti/j721e/evm.c @@ -71,8 +71,8 @@ int dram_init_banksize(void) #ifdef CONFIG_PHYS_64BIT /* Bank 1 declares the memory available in the DDR high region */ gd->bd->bi_dram[1].start = CONFIG_SYS_SDRAM_BASE1; - gd->bd->bi_dram[1].size = 0x80000000; - gd->ram_size = 0x100000000; + gd->bd->bi_dram[1].size = 0x40000000; + gd->ram_size = 0xC0000000; #endif
This made sure that conservatively the 1GB memory was reduced to account for Inline ECC.
So 4GB --> 3 GB.
Now since your available memory itself is 3 GB we can reduce it to 2.5GB.
Something like Below:
diff --git a/board/ti/j721e/evm.c b/board/ti/j721e/evm.c index d9846f3c46..8f4768f1a2 100644 --- a/board/ti/j721e/evm.c +++ b/board/ti/j721e/evm.c @@ -71,8 +71,8 @@ int dram_init_banksize(void) #ifdef CONFIG_PHYS_64BIT /* Bank 1 declares the memory available in the DDR high region */ gd->bd->bi_dram[1].start = CONFIG_SYS_SDRAM_BASE1; - gd->bd->bi_dram[1].size = 0x80000000; - gd->ram_size = 0x100000000; + gd->bd->bi_dram[1].size = 0x20000000; + gd->ram_size = 0xA0000000; #endif
Other parts should remain the same.
- Keerthy
Hi Nathan,
I have the enabled ECC for the higher addresses (> 32 bit addresses). Since
DJI the request is for 3GB ECC enabling. I have enabled 3GB DDR.
The R5 SPL cannot access > 32 bit addresses directly so it needs a Region based address translation.
(RAT) Mapping.
So While DDR gets initialized I map 0x80000000(Accessible by R5) to 0x880000000 (> 32 bits).
Clear them out to 0s. Unmap the RAT translation.
Set the ECC second range for the 3rd GB.
I have booted to Linux and memtester runs well.
More testing is welcome. Patch on top of 7.3.
0001-Enable-ECC-for-3-GB.patch
If no other questions please click on verify answer.
Best Regards,
Keerthy