Hi,experts
Use SD card, start A core and R core, use command soft connection, and find that R core is still running.
The default SD. A core runs, firmware runs, and other R core codes do not run.
Best Regards
Ti's customs
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,experts
Use SD card, start A core and R core, use command soft connection, and find that R core is still running.
The default SD. A core runs, firmware runs, and other R core codes do not run.
Best Regards
Ti's customs
version:ti-processor-sdk-rtos-j721e-evm-08_00_00_12
SD start: A core and R core
A core is loaded with ATF(Arm Trusted Firmware) at address: 0x70000000
MCU R5F is loaded with SPL/SBL at address 0x41C00000
If no other questions please click on verify answer.
- Keerthy
R Core in SD, MCU2_ 0,mcu2_ 1,mcu_ 3_ 1,mcu3_ 2. Four main domain cores are replaced by pdk8.0 demo according to different cores. These four cores and core a cannot be started at the same time (or successively)