Hello TI experts
I want to use the forward function of GMAC_SW to achieve the effect:
GMAC_SW has 3 port, one port is connected to CPPI bus(call it port-host), two ports are connected to PHYs(call it port-A and port-B).
when port-A(or port-B) received data, it can send data to port-host, then forward the data to port-B directly. The CPU host didn't take
part in the forward process, so it can reduce CPU overhead.
My question:
(1) if it can achieve the effect ?
(2) if it can, what I need to do ? if it is related with the driver of GMAC?