Hello,
We are using SDK 7.1 and Ethernet firmware fine for us. However 8 out of 10 times "ifconfig" or "ip link show" command is not working. This is the log
root@j7-evm:~# ping 192.168.1.208 PING 192.168.1.208 (192.168.1.208): 56 data bytes 64 bytes from 192.168.1.208: seq=0 ttl=64 time=0.346 ms 64 bytes from 192.168.1.208: seq=1 ttl=64 time=0.323 ms [ 35.888506] tlv71033: disabling 64 bytes from 192.168.1.208: seq=2 ttl=64 time=0.320 ms 64 bytes from 192.168.1.208: seq=3 ttl=64 time=0.337 ms ^C --- 192.168.1.208 ping statistics --- 4 packets transmitted, 4 packets received, 0% packet loss round-trip min/avg/max = 0.320/0.331/0.346 ms root@j7-evm:~# ^C root@j7-evm:~# root@j7-evm:~# root@j7-evm:~# root@j7-evm:~# root@j7-evm:~# root@j7-evm:~# ifconfig ^C^C^C^C
It works fine if we don't load the firmware built by TI RTOS and just build Linux SDK. We had to restart 8-9 times to get ifconfig or ip command working.
This is a big blocker for us. I would appreciate if we can get some help to resolve this issue.
Thank you,
Satish