Hi,
We used MMC0 for SD slot in our design.
Per check datasheet, the drive strength of MMC0_CLK is 6mA.
Could it be adjusted to more than 6mA?
Yume
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
No.
The IOs used in AM335x do not have drive strength control. There is a slew rate bit, but this bit must remain in the default state of fast for the device to be compliant to timing parameters defined in the datasheet.
Regards,
Paul