Dear experts,
Enviroment:sdk7.2+qnx710+custom board
In our custom board,csitx connect maxim96717F serializer.
I config csitx 1lane mipi,the data can be transmitted normal.
when I config csitx 2 lane mipi,serializer register value shows that 2-bit ECC error detected.
when I config csitx 4 lane mipi,serializer register value shows that HS sync pattern with 2 or more bit errors detected on data lane 1.
I try to change mipi data lane speed,the phenomenon is the same.
so I want to know is this hardware problem or software problem?
BR.