This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM368: Face Detection Option(Again)

Genius 4850 points
Part Number: TMS320DM368
Other Parts Discussed in Thread: DM385

Hi experts,

I understand that support for this device has been discontinued, but I would like to confirm the difference between products with and without "F" in the last model number.

Q1:Is it correct that the difference is whether or not the Hardware Face Detect Engine in the VPFE module is supported?

In DM385, there is a description as shown in the figure below, so I think it is the same.

Q2:Is it correct to assume that the software can be used as it is when migrating from a product without "F" to a product with "F"?
(We assume that sufficient evaluation is required.)

Best regards,
O.H