Hi
During production test of our custom AM5748 High Secure based CPU module it is sometimes helpful if the OTP tool would print-out some kind of message the the device has already been fused.
When the device is fused (OTP tool ran for the first time) there is output on UART3 which can be logged and checked for successful completion. But if the module has to be re-tested for some reason and the OTP tool is ran again, there is no output on UART3. Therefore it is difficult determine if there was a problem with fusing or another issue which prevents the module to start-up properly.
Thanks for your support.
Roger