Part Number: TMDS243GPEVM
Hi Team
My situation is summarized as follows:
Development board: tmds243gpevm
CCS version: v10.4.00006
Emulator: xds560v2
SDK version: MCU_ plus_ sdk_ am243x_ 08_ 00_ 00_ twenty-one
The problems encountered are as follows:
1. After 12V power supply, switch SW1 is turned to on, and the development board has no output of 5V and 3.3V. After using external 5V power supply to supply power to 5V test point and ground, the board has normal 5V and 3.3V output
2. At present, all programs cannot be downloaded, including the routines provided by Ti SDK. The download error information is as follows
MAIN_ Cortex_ R5_ 0_ 0: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x40: (Error -1065 @ 0x0) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration,
power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129)
MAIN_ Cortex_ R5_ 0_ 0: File Loader: Verification failed: Target failed to write 0x00000000
MAIN_ Cortex_ R5_ 0_ 0: GEL: File: F:\Am243x\J7_ V2\prj\app\Debug\app.out: Load failed.
A few days ago, I could download the program normally. During debugging, I pressed the reset button (SW4), the debugging was interrupted, and then the program could not be downloaded. During this period, there was no change in the program code and engineering configuration.
3. When DDR is used (after initializing DDR with gel file), the peripheral clock enable success signal cannot be obtained. Because it cannot be simulated now, the call stack cannot be provided. The specific implementation sequence is
SystemInit() ->PowerClock_ init() ->Module_ clockEnable() ->SOC_ moduleClockEnable() ->Sciclient_ pmGetModuleState() ->Sciclient_ service() ->Sciclient_ waitForMessage()
When entering sciclient_ After the waitformessage() function, the program falls into a loop waiting.
However, as long as DDR is not initialized with gel file, the same program runs normally.
I have two development boards in my hand. The situation of the two development boards is the same.
The main problems encountered now are the above three. Problems 1 and 3 can be avoided temporarily. The more urgent problem is problem 2. Please see what the problem will be and whether there are any solutions. Thank you.