Other Parts Discussed in Thread: AMIC110
I wrote a little BareMetal Project for the AMIC110_EVM_ICE board wich blinks some Leds.
I try to generate a Image from this elf binary.
To do so i did the following:
* I build my Project wich works fine if i deploy it over JTAG (XDS200)
* I ran this command line tool to generate an image: C:\ti\pdk_am335x_1_0_17\packages\ti\starterware\tools\ti_image\tiimage.exe 0x80001000 NONE BM_BlinkingLight.out BM_BlinkingLight_uart.bin
* I started TeraTerm wich receives 'C' characters. I then transfer the BM_BlinkingLight_uart.bin by using the XMODEM Protocol in TerraTerm.
After the transfer the Board no longer send characters.
I then connected the Debugger wich shows the CPU is stuck at: 0x0002008c. I assume this is some Interrupt?
It looks like the Boot Rom never jumps to the Start Address(0x80001000). This is also the Address that is configured inside the Target-configuration.