Other Parts Discussed in Thread: CSD
Hi Ti,
We are working on Linux SDK 07.01.00.18 on our customized board.
We have two eMMC solutions, one is ISSI IS21ES04G and another is Samsung KLM8G1GETF.
ISSI can work well, there is no problem. But Samsung cannot detect well.
In the below kernel log, I can only see "mmc1: new high speed SDHC card at address 59b4", but no mmc0.
Not sure if any dts setting need to be modified.
Could you provide some information about this?
Starting kernel ...
[ 0.000000] 000: printk: bootconsole [ns16550a0] enabled
[ 0.000000] 000: Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] 000: OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] 000: Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] 000: OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] 000: Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] 000: OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] 000: Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[ 0.000000] 000: OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] 000: cma: Reserved 24 MiB at 0x00000000be800000
[ 0.000000] 000: On node 0 totalpages: 110080
[ 0.000000] 000: DMA zone: 4096 pages used for memmap
[ 0.000000] 000: DMA zone: 0 pages reserved
[ 0.000000] 000: DMA zone: 247296 pages, LIFO batch:63
[ 0.000000] 000: DMA32 zone: 18446744073709414400 pages, LIFO batch:63
[ 0.000000] 000: psci: probing for conduit method from DT.
[ 0.000000] 000: psci: PSCIv1.1 detected in firmware.
[ 0.000000] 000: psci: Using standard PSCI v0.2 function IDs
[ 0.000000] 000: psci: Trusted OS migration not required
[ 0.000000] 000: psci: SMC Calling Convention v1.0
[ 0.000000] 000: percpu: Embedded 17 pages/cpu s32576 r8192 d28864 u69632
[ 0.000000] 000: pcpu-alloc: s32576 r8192 d28864 u69632 alloc=17*4096
[ 0.000000] 000:
[ 0.000000] 000: pcpu-alloc:
[ 0.000000] 000: [0]
[ 0.000000] 000: 0
[ 0.000000] 000: [0]
[ 0.000000] 000: 1
[ 0.000000] 000: [0]
[ 0.000000] 000: 2
[ 0.000000] 000: [0]
[ 0.000000] 000: 3
[ 0.000000] 000:
[ 0.000000] 000: Detected VIPT I-cache on CPU0
[ 0.000000] 000: CPU features: detected: ARM erratum 845719
[ 0.000000] 000: CPU features: detected: GIC system register CPU interface
[ 0.000000] 000: Built 1 zonelists, mobility grouping on. Total pages: 105984
[ 0.000000] 000: Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 isolcpus=1-3 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1m(ospi.sysfw),57216k@8m(ospi.rootfs),128k(ospi.phypattern) root=PARTUUID=9ffb92f1-02 rw rootfstype=ext4 rootwait
[ 0.000000] 000: Dentry cache hash table entries: 65536 (order: 8, 1048576 bytes, linear)
[ 0.000000] 000: Inode-cache hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.000000] 000: mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] 000: Memory: 930400K/440320K available (8446K kernel code, 612K rwdata, 3088K rodata, 1344K init, 417K bss, 18446744073709036960K reserved, 24576K cma-reserved)
[ 0.000000] 000: SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] 000: rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] 000: rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] 000: rcu: RCU priority boosting: priority 1 delay 500 ms.
[ 0.000000] 000: rcu: RCU_SOFTIRQ processing moved to rcuc kthreads.
[ 0.000000] 000: No expedited grace period (rcu_normal_after_boot).
[ 0.000000] 000: Tasks RCU enabled.
[ 0.000000] 000: rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] 000: rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] 000: NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] 000: GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] 000: GICv3: 960 SPIs implemented
[ 0.000000] 000: GICv3: 0 Extended SPIs implemented
[ 0.000000] 000: GICv3: Distributor has no Range Selector support
[ 0.000000] 000: GICv3: 16 PPIs implemented
[ 0.000000] 000: GICv3: no VLPI support, no direct LPI support
[ 0.000000] 000: GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[ 0.000000] 000: ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] 000: GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] 000: ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] 000: ITS@0x0000000001820000: allocated 524288 Devices @bc400000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] 000: ITS: using cache flushing for cmd queue
[ 0.000000] 000: GICv3: using LPI property table @0x00000000bcc30000
[ 0.000000] 000: GIC: using cache flushing for LPI property table
[ 0.000000] 000: GICv3: CPU0: using allocated LPI pending table @0x00000000bcc40000
[ 0.000000] 000: random: get_random_bytes called from start_kernel+0x2bc/0x440 with crng_init=0
[ 0.000000] 000: arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] 000: clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000001] 000: sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008993] 000: Console: colour dummy device 80x25
[ 0.014034] 000: Calibrating delay loop (skipped), value calculated using timer frequency..
[ 0.022669] 000: 400.00 BogoMIPS (lpj=800000)
[ 0.027127] 000: pid_max: default: 32768 minimum: 301
[ 0.032401] 000: LSM: Security Framework initializing
[ 0.037629] 000: Mount-cache hash table entries: 1024 (order: 1, 8192 bytes, linear)
[ 0.045559] 000: Mountpoint-cache hash table entries: 1024 (order: 1, 8192 bytes, linear)
[ 0.055538] 000: ASID allocator initialised with 32768 entries
[ 0.061622] 000: rcu: Hierarchical SRCU implementation.
[ 0.067477] 000: Platform MSI: gic-its@1820000 domain created
[ 0.073597] 000: PCI/MSI: /bus@100000/interrupt-controller@1800000/gic-its@1820000 domain created
[ 0.083050] 000: smp: Bringing up secondary CPUs ...
[ 0.089281] 001: Detected VIPT I-cache on CPU1
[ 0.093856] 001: GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[ 0.101343] 001: GICv3: CPU1: using allocated LPI pending table @0x00000000bcc50000
[ 0.109206] 001: CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.117653] 002: Detected VIPT I-cache on CPU2
[ 0.122243] 002: GICv3: CPU2: found redistributor 100 region 0:0x00000000018c0000
[ 0.129918] 002: GICv3: CPU2: using allocated LPI pending table @0x00000000bcc60000
[ 0.137797] 002: CPU2: Booted secondary processor 0x0000000100 [0x410fd034]
[ 0.146171] 003: Detected VIPT I-cache on CPU3
[ 0.150739] 003: GICv3: CPU3: found redistributor 101 region 0:0x00000000018e0000
[ 0.158409] 003: GICv3: CPU3: using allocated LPI pending table @0x00000000bcc70000
[ 0.166273] 003: CPU3: Booted secondary processor 0x0000000101 [0x410fd034]
[ 0.173538] 000: smp: Brought up 1 node, 4 CPUs
[ 0.178202] 000: SMP: Total of 4 processors activated.
[ 0.183481] 000: CPU features: detected: 32-bit EL0 Support
[ 0.189204] 000: CPU features: detected: CRC32 instructions
[ 0.204248] 000: CPU: All CPU(s) started at EL2
[ 0.208934] 000: alternatives: patching kernel code
[ 0.214891] 000: devtmpfs: initialized
[ 0.229072] 000: clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.239543] 000: futex hash table entries: 1024 (order: 5, 131072 bytes, linear)
[ 0.248233] 000: pinctrl core: initialized pinctrl subsystem
[ 0.254933] 000: NET: Registered protocol family 16
[ 0.261816] 000: DMA: preallocated 256 KiB pool for atomic allocations
[ 0.269234] 000: hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.295833] 000: HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.303197] 000: HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.310535] 000: HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.317853] 000: HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.326515] 000: cryptd: max_cpu_qlen set to 1000
[ 0.336529] 000: iommu: Default domain type: Translated
[ 0.342380] 000: SCSI subsystem initialized
[ 0.347440] 000: pps_core: LinuxPPS API ver. 1 registered
[ 0.352998] 000: pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.363063] 000: PTP clock support registered
[ 0.367562] 000: EDAC MC: Ver: 3.0.0
[ 0.372334] 000: FPGA manager framework
[ 0.377141] 000: clocksource: Switched to clocksource arch_sys_counter
[ 0.384147] 000: VFS: Disk quotas dquot_6.6.0
[ 0.388690] 000: VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.402332] 000: thermal_sys: Registered thermal governor 'step_wise'
[ 0.408946] 000: thermal_sys: Registered thermal governor 'power_allocator'
[ 0.416582] 000: NET: Registered protocol family 2
[ 0.422237] 000: tcp_listen_portaddr_hash hash table entries: 256 (order: 2, 16384 bytes, linear)
[ 0.431454] 000: TCP established hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.439890] 000: TCP bind hash table entries: 4096 (order: 5, 229376 bytes, linear)
[ 0.447986] 000: TCP: Hash tables configured (established 4096 bind 4096)
[ 0.455128] 000: UDP hash table entries: 256 (order: 3, 32768 bytes, linear)
[ 0.462426] 000: UDP-Lite hash table entries: 256 (order: 3, 32768 bytes, linear)
[ 0.470321] 000: NET: Registered protocol family 1
[ 0.475736] 000: RPC: Registered named UNIX socket transport module.
[ 0.482287] 000: RPC: Registered udp transport module.
[ 0.487565] 000: RPC: Registered tcp transport module.
[ 0.492830] 000: RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.499879] 000: PCI: CLS 0 bytes, default 64
[ 0.505455] 000: hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.518897] 000: Initialise system trusted keyrings
[ 0.524123] 000: workingset: timestamp_bits=46 max_order=18 bucket_order=0
[ 0.537845] 000: squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.545023] 000: NFS: Registering the id_resolver key type
[ 0.550694] 000: Key type id_resolver registered
[ 0.555482] 000: Key type id_legacy registered
[ 0.560055] 000: nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.567557] 000: 9p: Installing v9fs 9p2000 file system support
[ 0.587951] 000: Key type asymmetric registered
[ 0.592606] 000: Asymmetric key parser 'x509' registered
[ 0.598113] 000: Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.606172] 000: io scheduler mq-deadline registered
[ 0.611277] 000: io scheduler kyber registered
[ 0.618325] 000: pinctrl-single 4301c000.pinmux: 70 pins, size 280
[ 0.625343] 000: pinctrl-single 11c000.pinmux: 185 pins, size 740
[ 0.631891] 000: pinctrl-single 11c2e8.pinmux: 9 pins, size 36
[ 0.643409] 000: k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[ 0.650250] 000: k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[ 0.660906] 000: Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.680074] 000: brd: module loaded
[ 0.693258] 000: loop: module loaded
[ 1.070426] 000: libphy: Fixed MDIO Bus: probed
[ 1.075650] 000: tun: Universal TUN/TAP device driver, 1.6
[ 1.082033] 000: igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 1.090535] 000: igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.097107] 000: sky2: driver version 1.30
[ 1.102552] 000: VFIO - User Level meta-driver version: 0.3
[ 1.108715] 000: i2c /dev entries driver
[ 1.113866] 000: sdhci: Secure Digital Host Controller Interface driver
[ 1.120680] 000: sdhci: Copyright(c) Pierre Ossman
[ 1.126127] 000: sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.133713] 000: ti-sci bus@100000:bus@28380000:bus@42040000:dmsc: invalid resource
[ 1.142474] 000: optee: probing for conduit method from DT.
[ 1.148251] 000: optee: revision 3.8 (199fca17)
[ 1.153509] 000: optee: initialized driver
[ 1.158442] 000: NET: Registered protocol family 17
[ 1.163686] 000: 9pnet: Installing 9P2000 support
[ 1.168587] 000: Key type dns_resolver registered
[ 1.173888] 000: registered taskstats version 1
[ 1.178562] 000: Loading compiled-in X.509 certificates
[ 0.000000] 000: Booting Linux on physical CPU 0x0000000[ 1.196759] 000: k3-ringacc 2b800000.ringacc: Failed to get MSI domain
000 [0x410fd034]
[ 1.205871] 000: k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[ 1.216981] 000: ti-sci bus@100000:bus@28380000:bus@42040000:dmsc: invalid resource
[ 1.225316] 000: ti-sci bus@100000:bus@28380000:bus@42040000:dmsc: ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
[ 1.286489] 000: random: fast init done
[ 1.298781] 000: omap_i2c 42120000.i2c: bus 0 rev0.12 at 100 kHz
[ 1.305678] 000: omap_i2c 40b00000.i2c: bus 1 rev0.12 at 100 kHz
[ 1.312727] 000: omap_i2c 2000000.i2c: bus 2 rev0.12 at 100 kHz
[ 1.341284] 000: rtc-s35390a 3-0030: error resetting chip
[ 1.347203] 000: rtc-s35390a: probe of 3-0030 failed with error -5
[ 1.353629] 000: omap_i2c 2010000.i2c: bus 3 rev0.12 at 100 kHz
[ 1.360384] 000: omap_i2c 2020000.i2c: bus 4 rev0.12 at 100 kHz
[ 1.367118] 000: omap_i2c 2030000.i2c: bus 5 rev0.12 at 100 kHz
[ 1.373989] 000: ti-sci-intr bus@100000:bus@28380000:bus@42040000:interrupt-controller2: Interrupt Router 156 domain created
[ 1.385703] 000: ti-sci-intr bus@100000:interrupt-controller0: Interrupt Router 100 domain created
[ 1.395089] 000: ti-sci-intr bus@100000:navss@30800000:interrupt-controller1: Interrupt Router 182 domain created
[ 1.405942] 000: ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 179 created
[ 1.419621] 000: k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,32] sci-dev-id:195
[ 1.430008] 000: k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[ 1.437246] 000: k3-ringacc 2b800000.ringacc: RA Proxy rev. 66348100, num_proxies:64
[ 1.448334] 000: k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:818, gp-rings[304,100] sci-dev-id:187
[ 1.458920] 000: k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[ 1.466161] 000: k3-ringacc 3c000000.ringacc: RA Proxy rev. 66348100, num_proxies:64
[ 1.474880] 000: 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 8, base_baud = 6000000) is a 8250
[ 1.485114] 000: 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 19, base_baud = 3000000) is a 8250
[ 1.494369] 000: printk: console [ttyS2] enabled
[ 1.494369] 000: printk: console [ttyS2] enabled
[ 1.503735] 000: printk: bootconsole [ns16550a0] disabled
[ 1.503735] 000: printk: bootconsole [ns16550a0] disabled
[ 1.515476] 000: omap8250 2810000.serial: unable to register 8250 port
[ 1.515490] 000: omap8250 2810000.serial: PM domain pd:147 will not be powered off
[ 1.516203] 000: 2820000.serial: ttyS4 at MMIO 0x2820000 (irq = 21, base_baud = 3000000) is a 8250
[ 1.546176] 000: gen_74x164_probe enter...
[ 1.546329] 000: gpiochip_add_data_with_key enter..
[ 1.546337] 000: gpiochip_add_data_with_key name=gpiochip0
[ 1.546562] 000: gen_74x164_probe ret=0 [2]
[ 1.553576] 000: mdio name = 46000f00.mdio
[ 1.553582] 000: mdio name = 46000f00.mdio[1]
[ 1.593157] 000: davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 1.593170] 000: libphy: 46000f00.mdio: probed
[ 1.595120] 000: davinci_mdio 46000f00.mdio: phy[3]: device 46000f00.mdio:03, driver TI DP83822
[ 1.595155] 000: am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 quirks:00000000
[ 1.595634] 000: am65-cpsw-nuss 46000000.ethernet: Failed to request tx dma channel -517
[ 1.621240] 000: am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[ 1.621783] 000: thermal thermal_zone1: failed to read out thermal zone (-22)
[ 1.621811] 000: thermal thermal_zone2: failed to read out thermal zone (-22)
[ 1.622639] 000: mmc0: CQHCI version 5.10
[ 1.700270] 000: mmc0: SDHCI controller on 4f80000.sdhci [4f80000.sdhci] using ADMA 64-bit
[ 1.701314] 000: mmc1: CQHCI version 5.10
[ 1.721397] 000: mmc_attach_mmc mmc0
[ 1.772924] 000: mmc_attach_mmc mmc0
[ 1.820801] 000: mmc_attach_mmc mmc0
[ 1.880337] 000: mmc_attach_mmc mmc0
[ 2.691779] 000: mmc1: SDHCI controller on 4fa0000.sdhci [4fa0000.sdhci] using ADMA 64-bit
[ 2.701452] 000: gpiochip_add_data_with_key enter..
[ 2.701462] 000: gpiochip_add_data_with_key name=gpiochip1
[ 2.704659] 000: gpiochip_add_data_with_key enter..
[ 2.704669] 000: gpiochip_add_data_with_key name=gpiochip2
[ 2.708727] 000: gpiochip_add_data_with_key enter..
[ 2.708737] 000: gpiochip_add_data_with_key name=gpiochip3
[ 2.712162] 000: omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100
[ 2.712583] 000: omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100
[ 2.714326] 000: ti-udma 285c0000.dma-controller: Channels: 28 (tchan: 14, rchan: 14, gp-rflow: 16)
[ 2.726456] 000: ti-udma 31150000.dma-controller: Channels: 119 (tchan: 53, rchan: 66, gp-rflow: 64)
[ 2.733991] 000: mmc_add_card mmc1
[ 2.734001] 000: mmc1: new high speed SDHC card at address 59b4
[ 2.744166] 000: mmcblk1: mmc1:59b4 USDU1 28.3 GiB
[ 2.745635] 000: 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 20, base_baud = 3000000) is a 8250
[ 2.748050] 000: mmcblk1: p1 p2
[ 2.815191] 000: spi-nor spi9.0: unrecognized JEDEC id bytes: 00 00 00 00 00 00
[ 2.815217] 000: spi-nor: probe of spi9.0 failed with error -2
[ 2.816211] 000: mdio name = 46000f00.mdio
[ 2.816217] 000: mdio name = 46000f00.mdio[1]
[ 2.853156] 000: davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 2.853168] 000: libphy: 46000f00.mdio: probed
[ 2.853181] 000: call to get_phy_device addr=3 is_c45=0
[ 2.855132] 000: davinci_mdio 46000f00.mdio: phy[3]: device 46000f00.mdio:03, driver TI DP83822
[ 2.855166] 000: am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 quirks:00000000
[ 2.856845] 000: am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[ 2.861409] 000: am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 57.4
[ 2.861417] 000: am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 2.881237] 000: am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[ 2.896125] 000: debugfs: Directory 'pd:121' with parent 'pm_genpd' already present!
Thanks.
Eric