We are developing a custom application using the CDD IPC demo example provided, on MCU1_0 or MCU1_1.
we are not able to load the firmware onto the particular core, would like to know the steps to be followed to load the firmware onto the MCU cores on the MCU domain of Jacinto 7 EVM.
we tried replacing the DM_BOOT= / path to the new firmware and we ran the build to create tiboot3.bin, tispl.bin and u-boot.img(a_72).
6. Rebuild SPL and u-boot
6.1 cd PSDKLA_INTALL_PATH
6.2 make u-boot-r5_clean
6.3 make u-boot-a72_clean
6.4 make u-boot-r5
6.5 u-boot-a72
6.6 Replace the tiboot3.bin, tispl.bin and u-boot.img in the SD card BOOT/
after which we replaced these files on the SD card, unfortunately, the card doesn't boot up with the new files.