This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2SX: How to change the DDR memory size on the tda2?

Part Number: TDA2SX
Other Parts Discussed in Thread: TDA2,

Two DDRs are used in our own tda2 board, each of which is 2GB, with a total of 4GB.

It is found that the default memory node in DTS is 1GB. After changing it to 4GB, it is found that the kernel cannot be started. How can I use all 4GB of memory?

  • Hi,

    Can you please let me know on how you confirmed on the total of 4GB? Do you have a custom board or you are using standard TI TDA2SX EVM?
    The max that can be supported can be upto 4GB but I believe on the TI Board it is 2GB DDR. Can you share the links on 4GB DDR?

    Best Regards,
    Keerthy