I have some questions about the TensorFlow (https://www.tensorflow.org/overview/) for beginners tutorial (see code below).
(1) If I run this tutorial, as is, on the SK-TDA4VM, which processor will be used? The dual A72 or C7x?
(2) What is the workflow to convert this tutorial to use the TI EdgeAI-Model zoo pre-built models?
import tensorflow as tf
mnist = tf.keras.datasets.mnist
(x_train, y_train),(x_test, y_test) = mnist.load_data()
x_train, x_test = x_train / 255.0, x_test / 255.0
model = tf.keras.models.Sequential([
tf.keras.layers.Flatten(input_shape=(28, 28)),
tf.keras.layers.Dense(128, activation='relu'),
tf.keras.layers.Dropout(0.2),
tf.keras.layers.Dense(10, activation='softmax')
])
model.compile(optimizer='adam',
loss='sparse_categorical_crossentropy',
metrics=['accuracy'])
model.fit(x_train, y_train, epochs=5)
model.evaluate(x_test, y_test)