Hello,
Can I install a CSI-2 camera on the SK-TDA4VM, like a USB camera, can be used directly after it is installed?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can I install a CSI-2 camera on the SK-TDA4VM, like a USB camera, can be used directly after it is installed?
thanks
Hi,
I think so, but you would require fusion board and imx390 camera..
Regards,
Brijesh
你好,
I see from youtube that SK-TDA4VM provides CSI PORT.
Which is shown below.
Can I connect the CSI camera directly to the CSI2 PORT on the SK-TDA4VM?
Do I need to install the driver for CSI2 PORT or can I use it without installing the driver?
Regards,
Yi Fong
Hello Yi Fong,
Currently the SDK supports using OV5640 CSI camera module.
It is disabled by default, but can be enabled following the steps here: http://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-sk-tda4vm/08_00_01_10/exports/docs/getting_started.html?highlight=csi#ov5640-yuv-sensor. For this particular OV5640 CSI camera module used as an example, an external 5V power supply is required.
Regards,
Takuma
Hello,
The camera I use is from imagesource and driven by tiscamera.
After I installed the driver on SK-TDA4VM, an error occurred, as shown below.
Collected errors:
* Solver encountered 1 problem(s):
* Problem 1/1:
* - package tiscamera-tcamprop-0.1.0.armhf does not have a compatible architecture
*
* Solution 1:
* - do not ask to install tiscamera-tcamprop-0.1.0.armhf
And I refer to the webpage you provided, which mentions Camera sources (v4l2), and the camera source also uses GStreamer.
Does SK-TDA4VM not support the camera I am using?
The following webpage is the camera I am using.
https://www.theimagingsource.com/embedded-vision/mipi-csi-2-cameras/mipi-csi-2-board-cameras/dmm36mx297ml/
If it doesn’t work, can you provide me with a camera URL that is sure to be supported for my reference?
thanks
Regards,
Yi Fong
Hi Yi Fong,
package tiscamera-tcamprop-0.1.0.armhf does not have a compatible architecture
The architecture for the SK board, which can be found using the command uname -a, is aarch64 instead of armhf.
Does SK-TDA4VM not support the camera I am using?
Looking at the datasheet for your camera, the recommended operating voltage is 5V. The SK board outputs 3.3V from the CSI connector, so I don't think it is supported unless there is a way to supply external 5V power.
If it doesn’t work, can you provide me with a camera URL that is sure to be supported for my reference?
https://www.leopardimaging.com/product/cmos-sensor-modules/mipi-camera-modules/li-am65x-csi2 is used by TI, and it is a camera that needs an external 5V power supply. The documentation to get it up and running is here: http://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-sk-tda4vm/08_00_01_10/exports/docs/getting_started.html#ov5640-yuv-sensor
Regards,
Takuma