I build Vision SDK 3.08 on my custorm DRA722 board, when build ipu2 into vision sdk like:
PROC_IPU1_0_INCLUDE=no PROC_IPU1_1_INCLUDE=no PROC_IPU2_INCLUDE=yes PROC_A15_0_INCLUDE=yes PROC_DSP1_INCLUDE=yes
sample_app.out run ok , but it load firmware fail when enable IPU1 ( enable or disable IPU2 ) , linux startup log:
[ 16.988346] remoteproc remoteproc0: powering up 58820000.ipu [ 17.054634] remoteproc remoteproc0: Booting fw image dra7-ipu1-fw.xem4, size 3977424 [ 17.148958] omap-iommu 58882000.mmu: 58882000.mmu: version 2.1 [ 17.540473] remoteproc remoteproc0: bad phdr da 0x99000000 mem 0x4c8 [ 17.546899] remoteproc remoteproc0: Failed to load program segments: -22 [ 17.601720] remoteproc remoteproc0: failed to unmap 16777216/0 [ 17.607626] remoteproc remoteproc0: failed to unmap 16777216/0 [ 17.671042] remoteproc remoteproc0: failed to unmap 16777216/0 [ 17.837142] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2 ...
and run sample_app.out it will print "SYSTEM: Attaching to [IPU1-0] ..." , I need help ,thank you!