I have two TDA4 EVM boards. One is PROC078E8A, the other is PROC078E7A. And I use sdk to build tiboot3.bin sysfw.itb u-boot.img and tispl.bin and put these 4 files into MMC card. PROC078E8A didn't boot and PROC078E7A booted OK, I want to know what is wrong with the board and what I can do to solve the problem. The terminal printing which the board who didn't boot is
U-Boot SPL 2021.01-dirty (Oct 27 2021 - 02:10:32 -0700)
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E8
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
Trying to boot from MMC2
The terminal printing which the board who booted OK is
U-Boot SPL 2021.01-dirty (Oct 27 2021 - 02:10:32 -0700)
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E8
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
Trying to boot from MMC2
Starting ATF on ARM64 core...
NOTICE: BL31: v2.5(release):08.00.00.004-dirty
NOTICE: BL31: Built : 22:30:09, Aug 4 2021
U-Boot SPL 2021.01-dirty (Oct 27 2021 - 02:10:29 -0700)
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E8
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC2
U-Boot 2021.01-dirty (Oct 27 2021 - 02:10:29 -0700)
SoC: J721E SR2.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E8
DRAM: 4 GiB
Flash: 0 Bytes
MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Net: am65_cpsw_nuss_slave ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
eth0: ethernet@46000000
Hit any key to stop autoboot: 0