Hi
I'm trying to read the 8 channels of the ADC on an AMIC110ICE board. I know that the pins are not brought out to the outside world, but I was hoping to read at least some noise, but all the numbers coming out are identically 0. I doubt that's correct...
I have set up the steps to provide me with the step ID, and I am setting up one step for each of the 8 channels. My readout software correctly sees and decodes the step ID, but the data in it is all zeros. I'm thinking I have missed a setup step somewhere. I've modeled this after the starterware/examples/adc/volt_measure example. I've not enabled the interrupts to help simplify the process. Here is the code I use to iniitialize the ADC. When I check a ittle while after initializing, I have 4 words in each FIFO, and they have the tags. But no numbers where there should be numbers in the FIFO data. Thanks for any pointers!
void init_housekeeping()
{
int fifo, status;
tscAdcStepCfg_t adcStepCfg;
// power AFE up.
TSCADCAfePowerUp( TSCADC_BASE_ADDR );
/* Configure the ADC interrupts. */
// status = housekeeping_AdcIntrConfig(&data_ready);
// ADC clock divider register. AMIC110 is limited to 3 MHz. Let's use 2
TSCADCClkDivConfig( TSCADC_BASE_ADDR,TSCADC_MODULE_CLOCK,TSCADC_AFE_CLOCK);
/* Enable the step ID tag. */
TSCADCStepIdTagEnable(TSCADC_BASE_ADDR, TRUE);
/* Disable the write protection for Step config registers. */
TSCADCStepConfigProtectionEnable(TSCADC_BASE_ADDR, FALSE);
adcStepCfg.adcNegativeInpRef = TSCADC_NEGATIVE_REF_VSSA;
adcStepCfg.adcPositiveInpRef = TSCADC_POSITIVE_REF_VDDA;
adcStepCfg.adcNegativeInpChan = TSCADC_NEGATIVE_REF_VSSA;
adcStepCfg.adcPositiveInpChan = TSCADC_INPUT_CHANNEL1;
adcStepCfg.enableXppsw = FALSE;
adcStepCfg.enableXnpsw = FALSE;
adcStepCfg.enableYppsw = FALSE;
adcStepCfg.enableXnnsw = FALSE;
adcStepCfg.enableYpnsw = FALSE;
adcStepCfg.enableYnnsw = FALSE;
adcStepCfg.enableWpnsw = FALSE;
/* Enable ADC for GP mode. */
TSCADCTSModeConfig(TSCADC_BASE_ADDR, TSCADC_MODE_GP_ADC);
// Configure the steps, using the same step config for each
// Use FIFO 0 for channel 1-4, FIFO 1 for channels 5-8
for( int i = 1 ; i <= 8; i++)
{
adcStepCfg.adcNegativeInpChan = TSCADC_INPUT_VREFN;
adcStepCfg.adcPositiveInpChan = i;
TSCADCStepConfig(TSCADC_BASE_ADDR, i,
FALSE, &adcStepCfg);
TSCADCStepMode (TSCADC_BASE_ADDR, i,
TSCADC_STEP_MODE_SW_ENABLED_ONE_SHOT);
TSCADCStepDelayConfig(TSCADC_BASE_ADDR, i,SAMPLE_DELAY,OPEN_DELAY);
TSCADCStepIdTagEnable(TSCADC_BASE_ADDR,TRUE);
TSCADCStepSamplesAvg(TSCADC_BASE_ADDR, i,
TSCADC_SAMPLES_AVG_16);
if(i > 4)
fifo = TSCADC_FIFO_SEL_1;
else
fifo = TSCADC_FIFO_SEL_0;
TSCADCStepFifoConfig(TSCADC_BASE_ADDR, i,
fifo, FIFO_DEPTH_SETTING, FALSE);
//TSCADCFIFOIRQThresholdLevelConfig(TSCADC_BASE_ADDR, i,
// fifo, FIFO_DEPTH_SETTING, TRUE);
}
restart_housekeeping();
TSCADCEnable(TSCADC_BASE_ADDR, TRUE);
}
Here's the readout code:
void read_housekeeping_adcs()
{
int count,fifo,id;
uint32_t fifo_data;
// restart the conversions for next time.
UART_printf("Reading housekeeping ADC data...\r\n");
for( int i = 0; i < 2; i++ )
{
if ( i == 0 )
fifo = TSCADC_FIFO_SEL_0;
else
fifo = TSCADC_FIFO_SEL_1;
count = TSCADCGetFifoWordCount(TSCADC_BASE_ADDR,fifo);
while (count-- != 0)
{
// read the data out of the FIFO
// Decode the ID
// Decode the data and put it in the array
fifo_data = TSCADCGetFullFifoData(TSCADC_BASE_ADDR,fifo);
id = fifo_data >>16 ;
housekeeping_data[id] = fifo_data & 0xFFF;
UART_printf("C:%d id:%d hdta:%x data:%x\r\n ",count,id,housekeeping_data[id],fifo_data);
}
}
restart_housekeeping();
user_delay(10000000);
UART_printf("Done.\r\n");
}
Here's the screen output from a run:
Reading housekeeping ADC data...
C:3 id:0 hdta:0 data:0
C:2 id:1 hdta:0 data:10000
C:1 id:2 hdta:0 data:20000
C:0 id:3 hdta:0 data:30000
C:3 id:4 hdta:0 data:40000
C:2 id:5 hdta:0 data:50000
C:1 id:6 hdta:0 data:60000
C:0 id:7 hdta:0 data:70000