Hello
I use TMDSIDK574, CCS11, OS is Kubuntu 21 with kernel 5.13.0-20.
I try connect to the board using embedded usb XDS100v2 debug probe and every time it fails.
Error code is:
The value is '-604' (0xfffffda4).
The title is 'SC_ERR_LIB_ANY_LOAD'.
It can not load libjioserdesusb.so, but there is in the right directory.
By the way it works perfectly with CCS9, without any problem.
What is wrong with CCS11?
Thank you.