Hi
Customer would like to modify the SW (TI released SW for this product or customer's own SW) which was developed on "WindowsXP + CCS3.x" now.
Are they able to do it on "Wondows10 + latest CCS"?
Thanks and Best regards,
Tsurumoto.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Customer would like to modify the SW (TI released SW for this product or customer's own SW) which was developed on "WindowsXP + CCS3.x" now.
Are they able to do it on "Wondows10 + latest CCS"?
Thanks and Best regards,
Tsurumoto.
Tsurumoto,
The answer is yes but it may not be easy.
There are a number of things to consider:
The easiest path would be to run a Windows XP VM on Windows 10 and use CCSv3.x in that environment. However if they do want to move to CCSv11 it is possible but will require effort.
Regards,
John
Here are more details on the project migration.
https://dev.ti.com/tirex/explore/node?node=ANA-2UvaDVeIvwRHD7a0Sw__FUz-xrs__LATEST