Other Parts Discussed in Thread: TDA4VM
When trying to use the SK-TDA4VM to compile the model, using the following code, provided in the "Edge AI Academy":
tidl_delegate = [tflite.load_delegate(os.path.join(os.environ['TIDL_TOOLS_PATH'], 'tidl_model_import_tflite.so'), compile_options)]
I get the error: tidl_model_import_tflite.so: cannot open shared object file: No such file or directory
It seems the TIDL tools is not installed in the image file downloaded: ti-processor-sdk-linux-sk-tda4vm-etcher-image.zip version 08.00.01.10. Search the complete filesystem and the file is not there.
I checked some documentation for the installation, but it is not clear at all, because it assume a lot things instead of providing step by step how to download it and install it. I would like to be able to compile
custom model using SK-TDA4VM (Linux Ubuntu) and/or Windows10, I do not want to depend of the TI Edge AI Cloud. How can I do it ?
I repeat it, again, I checked some documentation and it is not clear or assume too much as follow:
Setting up the environment
TIDL is installed by SDK installation and can be found inside ${PSDKRA_PATH}/tidl_j7_01_00_00_00
. Run the following steps to export required variables and install tools for ease of use.
For Linux Users
Export the path of TIDL root directory as
TIDL_INSTALL_PATH
. All examples in this guide will use paths and filenames relative to this directory.user@ubuntu-pc$ export TIDL_INSTALL_PATH=${PSDKRA_PATH}/tidl_j7_01_00_00_00
There is not variable PSDKRA_PATH or TIDL_INSTALL_PATH and there is not directory tidl_j7_01_00_00_00 in the whole filesystem.
Any help is welcome. I am trying to compare this product with Nvidia Jetson Nano.