thirdparty Application need the openssl lib‘ version is v1.1.1
But openssl is v1.0.2 in PLSDK,we need upgrade openssl to v1.1.1.
Do you have any patches for v1.1.1 openssl to support Jactinto 6?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
thirdparty Application need the openssl lib‘ version is v1.1.1
But openssl is v1.0.2 in PLSDK,we need upgrade openssl to v1.1.1.
Do you have any patches for v1.1.1 openssl to support Jactinto 6?
Hi,
The openssl upgrades come as part of the oe-core layer.
PSDKLA 3.04 is based on krogoth branch and this comes with the support of openssl 1.0.2.
However, TI also made an updated release PSDKLA 6.00.00.03 (http://downloads.ti.com/infotainment/esd/jacinto6/processor-sdk-linux-automotive/6_00_00_03/index_FDS.html) which is based on yocto thud branch, this version of the Yocto/oe-core has the openssl version 1.1.1.
You can use this as a reference to port the openssl version to the PSDKLA 3.04.
Note that we expect this to have multiple dependencies with the oe-core. TI does not have plans to do this port. Also, we have not got this request/done this work for any customer. Please continue this implementation using the above pointers.
Regards
Karthik