Hi experts, we are planning to use ICSSG as realtime ethernet ports under RTOS which TTS function is a must. So we plan to port TTS from AM65X or AM57X to AM64X SDK. But we have to problem here.
1. Where can we find the source code of ICSSG dualmac source code from AM64 SDK?(now looks like we can only get plain text bin data file inside the SDK package)
2. Is ICSSG inside AM64X and AM57X very the same? Can we use the firmware code from AM65X or AM57X as the base, then verify and do some minor change on the source code, then test it on AM64X. Is this possible?
3. Other better suggestions?