Other Parts Discussed in Thread: AM5728
Dear Team,
We read the TRM of am5718 for a camera specific problem.
It is said on page 128 of TRM:-
If the CTRL_CORE_VIP_MUX_SELECT[6:4] VIP_SEL_1A bit field is set to 0x1 (GROUP5A pads) the
vin1a_clk0 signal can be mapped to the gpio6_10 device pad after the
CTRL_CORE_PAD_GPIO6_10[3:0] GPIO6_10_MUXMODE bit field has been set to 0x9.
We are using group5a pad for vin1a port.
But if check the Table 18-1054. CTRL_CORE_VIP_MUX_SELECT
at address 0x4A00 2E8C (ie using devmem2 0x4A00 2E8C)
we get 0x0000000.
Our question is, does VIP or any other driver set that register address indeed.
We also cross examine for am5728 TRM there is not any CTRL_CORE_VIP_MUX_SELECT.
We are able to capture on vin1a port if the SOC is am5728 but failed to perform same with am5718 SOC.
So any difference in the driver (VIP, VPDMA) configuration for both SOC?
Regards
Krishna Vashistha