Part Number: TDA2HG
Hi team,
The chip used by the Soc is the TDA2x, and the dp83tc811r used by phy, which communicates through the rgmii mode.
1. The customer intends to set the TX_CLK divider of the TDA2x to change its frequency to 25 Mhz (current frequency is 500 Mhz), modified the value of register 0x4a0052c0 and found a change in the TX_CLK frequency.
If the customer would like to do the same through configuring dts, what should be done?
2. It was also found that the current Soc state is In-band state, causing the rgmii mode to be "10 Mbps/Half - flow control off" anyway. Is there a lack of what kind of handshake between the Doc and the phy then cause In-band state? Could you also provide the timing of the interaction between the soc and the phy?
Could you help check the question above? Thanks.
Best Regards,
Cherry