Now that I have been able to... 1) Build and modify the IBL 2) Use the writing tools to load the IBL into the EEPROM. Now I would like to see a CCS project that is properly configured to build and create an image that can be loaded into the SPI flash. Is there an example project like this available? (like the UART example that your boot listing from my previous question showed.)