HI All,
I want to run the weston clinet demo on the J7 TDA4 and DP displays according to
software-dl.ti.com/.../Graphics_and_Display.html
but I get following errors in modetest command
1、root@j7-evm# modetest -M tidss -c
failed to open device 'tidss': No such file or directory
2、when launch Weston,with --tty-1 and without --connector argument, I get following error
root@j7-evm:/etc/init.d# weston --tty=1
Date: 2021-11-30 UTC
[03:01:53.854] weston 8.0.0
wayland.freedesktop.org
Bug reports to: gitlab.freedesktop.org/.../
Build: 8.0.0
[03:01:53.854] Command line: weston --tty=1
[03:01:53.854] OS: Linux, 5.4.106-00004-g31e5a020266e-dirty, #4 SMP PREEMPT Fri Dec 10 07:51:47 UTC 2021, aarch64
[03:01:53.854] Using config file '/etc//weston.ini'
[03:01:53.854] Output repaint window is 7 ms maximum.
[03:01:53.854] Loading module '/usr/lib/libweston-8/drm-backend.so'
[03:01:53.857] initializing drm backend
[03:01:53.857] logind: failed to get session seat
[03:01:53.857] logind: cannot setup systemd-logind helper (-61), using legacy fallback
[03:01:53.857] no drm device found
[03:01:53.857] fatal: failed to create compositor backend
Internal warning: debug scope 'drm-backend' has not been destroyed.
Can anybody help me to figure out these problem?
Thanks in advance,