Other Parts Discussed in Thread: OMAP-L138
Hello
I will use 66AK2G12 for the new project, so i'm testing it using the EVMK2G board.
I have experience in product development using OMAP-L138. When using the L138, i used the DSP Starterware included in the RTOS-SDK to develop in the baremetal environment of the C6748.
Basic booting was successful using the MLO file in the sd-card of EVMK2G. From now on, i'm going to proceed with the development using only the DSP of 66AK2G12. The ARM processor is planning to use Linux later, and now i'm going to develop it in a beremetal environment using only the DSP C66x.
Is the Starterware provided by L138 SDK not provided by 66AK2G12? The example built by PDK seems to be made for RTOS, and there is no problem with execution. However, various errors occur when compiling an example inside the CSL folder.
I am looking for example projects and methods of using low level drivers that can be used in DSP's Beremetal environment.
I look forward to hearing from someone who can help me.